8/15/2024 6:14 PM | |
Joined: 4/5/2024 Last visit: 8/21/2024 Posts: 1 Rating: (0) |
Hello everyone, I'm using a SCADA software called "Scada BR" to collect data from a 7SR511 protection relay. My main goal is to display real-time current readings by retrieving the current meter values from the relay’s input registers. However, every time I attempt to read one of these input registers with my SCADA system, I receive the following error message: "Illegal data address." The basic configurations have been completed, and my SCADA software is able to detect the relay, so there is some level of communication. However, I can't understand why I'm receiving this error when the address I'm using seems correct. Could someone please assist me in resolving this issue? Thank you in advance! Attachment7SR5_Communication_Protocol_Manual_V2.40.zip (44 Downloads) |
Last edited by: isaias_junior163 at: 08/15/2024 18:19:53 |
|
Follow us on