7/25/2023 10:20 AM | |
Joined: 4/30/2023 Last visit: 2/6/2024 Posts: 33 Rating:
|
anyone can help me with this ? |
7/25/2023 8:26 PM | |
Joined: 4/28/2015 Last visit: 7/11/2024 Posts: 43 Rating:
|
Seems strange, the description of the parameter says: And 10101 doesn't seem to fit the description of the parameter. Just a thought, did you connect +24V to pin 1 and common to pin 10? Also, if you haven't seen it, all documentation for the 808 is available at https://support.industry.siemens.com/cs/ww/en/view/109780845
|
7/26/2023 8:36 AM | |
Joined: 4/30/2023 Last visit: 2/6/2024 Posts: 33 Rating:
|
Hi Steve kudos to you, looks like you know where novice will fail. I def read the line about using external power supply, however it says (" For the probe, use an external voltage (24 V) whose reference potential should be connected to X21 pin 10 ") nothing about connecting 24v to pin 1. another question. can I use the same power supply which is connected to CNC itself or I have to add another one(limited space in the box) ? regards
|
Follow us on