1/22/2018 8:45 AM | |
Joined: 4/22/2015 Last visit: 5/18/2024 Posts: 4 Rating: (0) |
I have a very similar issue on an 840D with axis 4 & 5 on same amplifier. Complete amplifier change, both motors, both encoder cables changed same result. False temperature readings then unit will start getting correct readings. The motors are cool to the touch but read 190°C. Is it possible to mask out alarms 300613 and 300614 so the machine can be operated? We cannot afford the nuisance faults at this time. Attempted to mask out at MD1601 but alarms were still occurring. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 1/22/2018 2:29:03 PMNew subject after splitting |
|