5/28/2019 10:05 AM | |
Posts: 4 Rating: (0) |
Hello, Hope anybody can help, Have 840D sl with X130 connected to factory network for using OPC UA. IP address and network setup has been set, shows correctly on HMI, I can ping the machine, get access to the machine via SSH (port 22) and VNC (port 5900), but not via OPC UA. Test license has been set, basesys.ini shows open ports: FirewallOpenPorts=TCP/4840 TCP/102 TCP/5900 TCP/22 OPCUA option is enabled, username password is set Different OPC UA Clients are used, with and without username/password for authentication, but all fail to find the machine. CMC software version 4.7 SP4 From network prespective there is no firewall between my laptop and the machine, but unable to connect to the machine. Any idea's or similar experiences? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/28/2019 14:16:57New subject after splitting Last edited by: PeterKLM at: 06/04/2019 14:03:02 |
|