Industry Online Support
Technical Forum
1/28/2008 2:14 PM | |
Posts: 15 Rating:
|
Hi SteveJ PLC is running and there is no fault on PLC all other input and output is working i can see them in S7 program.This is a new startup. I can not configured in the MCP in plc H/w. Because i have not seen any OP032s gsd file in H/W library. There are two led behind op032s and one of them is green means power is ok. The other one is connection led but it is flashing. Maybe attached.xls file help you to solve my problem. Best Regards Attachmenthw.zip (332 Downloads) |
Follow us on