10/8/2012 11:14 PM | |
Joined: 1/19/2008 Last visit: 8/12/2024 Posts: 988 Rating: (63) |
Hi, If the system sees the adi4 then set up the equidistant DP cycle. Pee |
10/12/2012 2:40 PM | |
Posts: 25 Rating: (0) |
2nd Screen |
10/12/2012 2:42 PM | |
Posts: 25 Rating: (0) |
3th Screen |
10/12/2012 6:24 PM | |
Posts: 25 Rating: (0) |
Hello Pee El Sea, DP Baudrate is 12Mb. When Save and Recompile all, there is no error. On the same Profibus network there are also 1 CU320DP and 1 CU310DP and 1 PP72/48. All that communication without any problem. I can move motors in scout by commisioning. But ADI4 dosent communication. H1 LED is Green, H2 LED is Red. Please take a look my project. Thank you very much for interesting. Attachment840dis_1.zip (161 Downloads) |
10/14/2012 1:44 PM | |
Joined: 1/19/2008 Last visit: 8/12/2024 Posts: 988 Rating: (63) |
Hi, Can you connect your programmer onto the profibus line and look in diagnostics and see the adi4 card ? Pee |
Follow us on