2/28/2024 6:21 PM | |
Joined: 2/27/2024 Last visit: 4/3/2024 Posts: 1 Rating: (0) |
Hello, like some other folks I'm trying to connect my Siemens S7-1200/1214C with MQTT broker on a RaspberryPi but there is 8601 error. I'm using this: Libraries for Communication for SIMATIC Controllers Entry ID:109780503 Under the "typeDiagnostics" I see 80C5. When I look it up in the "Information system" as: "TSEND_C: Establishing a connection and sending data", I can see the error there as the following: - Connection terminated by the communication partner. - LSAP of the remote connection partner is not released. - See also the description of STATUS 16#80C5 for TCON (I don't know where to see this..) I found this youtube video and followed it and still get 8601. I tried the LHTTP block.. but get the same error 8601. I think it has something to do with the internet set up in the PLC?
|
2/28/2024 6:35 PM | |
Joined: 12/18/2014 Last visit: 6/2/2024 Posts: 33140 Rating: (4094) |
Please don't post twice for the same problem. |
2/29/2024 11:16 AM | |
Joined: 8/21/2014 Last visit: 5/24/2024 Posts: 959 Rating: (13) |
Closed cause question posted twice. The second thread with the subject Error 8601 when using libraries for communication is published within the conference Communication / Networks Best regards, |
My Forum is the place to personalize your profile, |
|
Follow us on