7/8/2013 11:17 AM | |
Posts: 241 Rating: (50) |
this link might help u http://support.automation.siemens.com/WW/view/en/37706606 |
7/8/2013 1:46 PM | |
Joined: 11/21/2007 Last visit: 7/7/2024 Posts: 2325 Rating: (307) |
Thanks TechTeam Do I also have to Enable External Encoder like it is in the Material Axis ? Cheers Navnag |
There is no such thing as the last bug in a program |
|
7/8/2013 2:18 PM | |
Posts: 344 Rating: (50)
|
Yes, Extrernal Encoder Technology Object must be enabled just like Axis Technology Object. All Technology Object have a corresponing _enableXxxx() command. |
Follow us on