7/8/2013 5:36 PM | |
Joined: 3/18/2008 Last visit: 12/8/2023 Posts: 1750 Rating: (272) |
Hello, Here is the Procedure in attachment. Best of luck Attachmentwincc_redudancy.zip (1732 Downloads) |
VANDE MATARAM..... |
|
This contribution was helpful to1 thankful Users |
7/8/2013 5:48 PM | |
Joined: 2/20/2010 Last visit: 7/9/2024 Posts: 104 Rating: (7) |
There is ready made wizard script you have run to make redundancy in wince named with "redundant connection". |
10/23/2013 12:38 PM | |
Joined: 4/24/2009 Last visit: 8/20/2024 Posts: 2682 Rating: (135) |
New question splitted to Redundancy via comercial ethernet cards and sofware redundancy 315-2 dp Best regards O_Moderator |
This contribution was helpful to1 thankful Users |
11/9/2017 7:19 PM | |
Joined: 9/1/2005 Last visit: 8/12/2024 Posts: 4104 Rating: (195) |
New question published by manhar71 is split to a separate thread with the subject add two CP's 443-1 to a redundant system consisting of two cpu's (412-5H PN/DP). Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on