12/21/2007 8:30 AM | |
Joined: 5/25/2007 Last visit: 8/8/2024 Posts: 83 Rating:
|
Dear Sir: I have a problem about S7 317-2dp with 512kb MMC. CPU->6ES7317-2AJ10.0AB0 v2.1.3 MMC->6ES7953-8LJ20-0AA0 (1)Iplugged the 128kb mmc card in CPU317-2dp,it runs ok. (2)I plugged the 512kb mmc card in CPU317-2dp,the stop led of the cpu always flash (3)I Put the switch to Res, until the flashing differs (can last 10 seconds) then release switch and put it back to Res within 3 seconds. Hold it for more than 5 seconds. the stop led of the cpu always flash (4)I format it in PC then plug in CPU,do overall reset,the same situation. (5)change other new 512k mmc,the same situation. what do I watch out this? Best regards BuzzLightYear TEL:+886-2-29995926 FAX:+886-2-29995929 Mobile Phone:+886-932018640 E-Mail Address: <mailto:vincentchang@anpro.com.tw> 5F/9,NO.14,Lane 609,Sec.5,Chung Hsin Rd, San Chung City,Taipei County,Taiwan,R.O.C |
12/21/2007 9:31 AM | |
Joined: 8/31/2005 Last visit: 7/18/2024 Posts: 2198 Rating:
|
If you formated the MMC with Windows you can not use it with SIMATIC anymore. Look here: http://support.automation.siemens.com/WW/view/en/19515769 |
|
|
12/24/2007 1:54 AM | |
Joined: 5/25/2007 Last visit: 8/8/2024 Posts: 83 Rating:
|
Dear Miami: Buzz LightYear |
3/6/2008 11:25 PM | |
Posts: 14 Rating:
|
Hi If you want to format the MMC, you have two options: using a prommer or format directlyfor S7-300CPU. Use a external promer check the next link: http://support.automation.siemens.com/WW/view/en/21829579 Format or reset an MMC (Micro Memory Card) for SIMATIC S7-300 CPUs, check link: http://support.automation.siemens.com/WW/view/en/21830698 I hope this information help you. |
Follow us on