4/27/2023 7:59 AM | |
Joined: 3/26/2023 Last visit: 7/1/2024 Posts: 7 Rating: (0) |
Hello everyone. Therefore: We have a Tank1 with a water level Probe1 that gives one of 4 states, A or B or C or D. We have a Tank2 with a Water Level Probe2 that gives one of 4 states, A or B or C or D. We have 1 pump that pumps water into those 2 tanks. In Condition table (in attach) in rows 6 and 12 we have an example of conflict. 6th row: Tank1 A and Tank2 (A or B or C or D) and FULL = Pump OFF. 12th row: Tank1 (A or B or C or D) and Tank2 C and FULL = Pump ON. The problem is that the pump cannot be ON and OFF at the same time. The problem is also that the Condition table says that in row 6 the state of Tank2 is "no influence", but Tank2 actually has influence because it has one of 4 states (A, B, C, D). Attached is the Condition table and the basic project (in next post) set up in LSC. How to adjust the system so that all conditions are met, and there are no conflicts? Is that possible. What do you think? Thank you. AttachmentCondition table.xlsx (328 Downloads) |
Last edited by: Dardem at: 04/27/2023 08:04:09Last edited by: Dardem at: 04/27/2023 08:08:15Last edited by: Jen_Moderator at: 04/27/2023 12:17:51Text formatting optimized. |
|
4/27/2023 8:00 AM | |
Joined: 3/26/2023 Last visit: 7/1/2024 Posts: 7 Rating: (0) |
Project. AttachmentPump with two tank-forum.zip (335 Downloads) |
Follow us on