6/27/2010 12:11 PM | |
Joined: 9/18/2006 Last visit: 7/13/2024 Posts: 589 Rating:
|
Hi. I assume, that you can use FB83 for the decision of your problem. FB83 Contains calls SFC14 and SFC15. The forum has many thread for the information on work FB83. It can to you will help. https://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&lang=en&objid=10804940&subtype=133100&caller=view https://www.automation.siemens.com/tf/WW/en/Posts/44633#top Best regards. |
6/27/2010 5:39 PM | |
Joined: 10/7/2005 Last visit: 7/22/2024 Posts: 3010 Rating:
|
Hello chetan747 your ABB drive is meant support the PROFIdrive profile which means you should be able to read and/or writeparameters via Dataset 47 (DS47) requests (the PROFIdrive profileis standardised by PI andif you are a member of PI you can download it from HERE). You can use either SFC58/59 or SFB 52/53 in your S7 todo an acyclic DS47 related request and examples how this is done with Siemens drives can be found HERE(not done in CFC, but you can of course do the SFC or SFB calls in CFC too). I suggest you first check with ABB to ensure that your Drive really supports PROFIdrive related DS47 requests before you go through the trouble of programming these. I hope this helps |
Cheers |
|
This contribution was helpful to
2 thankful Users |
7/1/2010 3:27 PM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating:
|
Hello, So, sorry for delay. Best regards, Hristo Mihalev AttachmentAbb.zip (1903 Downloads) |
Last edited by: UMENCHO at: 7/1/2010 3:28 PM |
|
This contribution was helpful to
2 thankful Users |
11/2/2010 10:17 AM | |
Joined: 9/6/2008 Last visit: 5/7/2022 Posts: 1121 Rating:
|
HI Umencho Can you please convert your program of ABB drive to english as i not able to open it. |
Jazz |
|
12/5/2010 9:20 PM | |
Joined: 11/1/2009 Last visit: 7/7/2024 Posts: 9 Rating:
|
Ekteki programda kontrol fonksiyonu verilmistir. Kontrol icin PPO 4 kullanildi. Fonksiyonun ozelligi, ek bir DB yada UDT kullanilmadan All-in-one mantigi ile herseyi icerinde bulundurmasi. PZD alanini okumak icin; Driverin hangi parametresi okunmak isteniyorsa, Parametre 51.06 'dan itibaren Driver uzerinde tanimlanmasi gerekiyor. Gerekli Aciklamalar Fonksiyon icerisindedir. ---------------------------------------------------------------------------------------------------------------------------------------- ABB RPBA01 Control Function give at attachment. I use PPO 4 for Driver Control. This Function is All-in-one; along it function working without any DB or UDT. Read for PZD area; You must parameters settings on the Driver. PZD Settings Area begin from Parameter 51.06. Needed definition, inside of function. ihsan KAYMAN AttachmentABB_RPBA.ZIP (1639 Downloads) |
This contribution was helpful to
11 thankful Users |
Follow us on