Industry Online Support
Technical Forum
5/5/2008 11:47 AM | |
Joined: 9/27/2006 Last visit: 8/16/2024 Posts: 12277 Rating: (2680) |
Hello obyone_2; It would help to know which As-i module you plan to use, we could look at datasheets on the web. That being said, there are only 2 wires on As-i, one 24 V, the other (-). Shouldn't be too hard. If thee are 4 terminals, 2x24V and 2x (-) are looped, so you can use them as incoming and outgoing. What cable are you planning to use uin your application? Yellow As-i flat cable? How are you planning to address the slave modules? Modules come in various connection sizes, generally in multiples of 4: 2 IN/2 OUT, 3 IN/1 OUT, 4 In/4 OUT, 8 IN/8 Out...Have a look at www.as-interface.net/Products Come back to us for more detailed questions, Hope this helps, Daniel Chartier |
5/5/2008 3:44 PM | |
Joined: 9/27/2006 Last visit: 8/16/2024 Posts: 12277 Rating: (2680) |
Hello obyone_2; The As-i power supplies that I have worked with have screw terminals for connection to the As=i bus; we would simply remove some of the insulation of the As-i cable and wire the cable onto the terminals. By the way, you'll need to do the same at the other end of the cable to connect the Cp243-2 As-i master. I am attaching an illustration of the As-i bus showing this. It is from the CP243-2 manual, in case you do not have it handy. http://support.automation.siemens.com/WW/view/en/2659515 There also is a self-extracting file available with program examples for Microwin: http://support.automation.siemens.com/WW/view/en/2659515 Attaching the yellow As-i cable to the slaves is easy, the cable is profiled and can be setup easily in only one position on the slave. Sometimes there are requirements for another cable, for output power, if required, and the power available on the standard cable is not sufficient. We learned this when we started wondering why our outputs were not turning on??? . Hope this helps, Daniel Chartier |
Last edited by: O_Moderator at: 9/16/2010 3:06 PMlink edited |
|
Follow us on