11/27/2010 2:57 PM | |
Posts: 69 Rating: (1) |
DEAR SIR, I am retrofiting one boring machine with 840d system, The machine having 6 axes and one spindle, X,Y,Z, W,B,A ,SP All AXEOS motor encoder are absolute. All external encoder are absolute encoders. X,Y,W axes connected with linear scale Absolute, make: heidenhain. Z,A,B axes are connected with Rotary Encoder, make :heidenhain, 2048 ppr, ROC413, endat01 External encoder Z and A AXIS.Reference position lost every time power off and on, Reference Symbol showing and 34210 ENC_REFF_STATE == 2 showing. I changed external encoder cable , there is no improvement. I changed axes control card on drive side , then there is no improvement. Kindly help me to slove the problem. NCU: 572.5 HMI:6.4 ROTARY ENCODER DETAILS ************************************** MAKE: HEIDENHAIN ROC 413 RESOLUTION :2048 ENDAT01
regards, Balaji AttachmentNC_17_11_2010.pdf (80 Downloads) |
Follow us on