7/28/2016 10:02 AM | |
Joined: 12/23/2011 Last visit: 11/22/2022 Posts: 143 Rating: (0) |
hi do you can connect this Accelerometer sensor to analouge input module? the pdf file attach. thanks AttachmentA3 ACC10-20_Brochure - rev1.pdf (433 Downloads) |
7/29/2016 6:35 PM | |
Joined: 12/23/2011 Last visit: 11/22/2022 Posts: 143 Rating: (0) |
thanks yes i have analouge card siemens. |
7/30/2016 7:51 PM | |
Joined: 12/23/2011 Last visit: 11/22/2022 Posts: 143 Rating: (0) |
the code is 6ES7331-7KF02-0AB0 |
12/24/2016 12:52 PM | |
Joined: 12/23/2011 Last visit: 11/22/2022 Posts: 143 Rating: (0) |
hello very thanks for reply we Having a separate board PID for this sensor but We want THIS sensor connecting directly to the analog card PLC. IF WE CONNECT THIS SENSOR TO ANALOG PLC: HOW configure this sensor for (10 g or 20 g) because programmable by board(REG 10-20)?? It is important configure 10 g or 20 g?? NOTE:this sensor install on the ELECTROMAGNETIC Vibrating FEEDERS AttachmentA2 REG10-20_Brochure - rev1.pdf (332 Downloads) |
Last edited by: PLC2011 at: 12/24/2016 7:37:12 PM |
|
Follow us on