9/6/2021 12:16 PM | |
Joined: 11/8/2018 Last visit: 5/22/2024 Posts: 84 Rating: (0) |
Good Morning, I have a logo 8.2 (6ED105-1Md08-0BA0) and I have setted the LWE and have entered on the web true connected internet cable true the web login. The i had to install it on a movable equipment and bought the CMR 2020. I managed to set the CMR2020 and i am pinging to the CMR2020. when I go in the browser I also log on the CMR2020. But when I come to ping the logo ip address or enter the ip address in the web browser it is not working. Is there some one so kind that can guid me if there is a particular job that i need to do or do i have to upgrade to CMR 2040 as it is working very slow? could it be that the logo needs to be v8.3 instead of 8.2 Thanks Mark Paul AttachmentCMR2020.zip (227 Downloads) |
Last edited by: MPBusuttil at: 09/10/2021 11:08:26Last edited by: MPBusuttil at: 09/10/2021 11:25:58Last edited by: MPBusuttil at: 09/10/2021 11:28:54 |
|
Follow us on