11/13/2006 6:57 PM | |
Posts: 1084 Rating: (72)
|
Looks to me that you have more then 5000 actions running at the same time. |
11/14/2006 10:20 AM | |
Posts: 3149 Rating: (171)
|
Hi perhaps this FAQ can help as well http://support.automation.siemens.com/WW/view/en/2357302 nemo |
11/14/2006 11:47 AM | |
Posts: 1084 Rating: (72)
|
Thanks Nemo, I have a day off I think, forgot even to look in the faq myself... with regards, Ikkezelf |
11/14/2006 12:05 PM | |
Joined: 3/8/2006 Last visit: 7/9/2024 Posts: 15 Rating: (4) |
Sorry I didn't take the log file, but as I can see, there was no special message in it. If you really need them, I can ask my customer to send them to me. I don't know if it could help, but in the WinCC application there is an action with notrigger. Normally this action should not be activated, but does the system always used it ? To answer Nemo,the FAQ "http://support.automation.siemens.com/WW/view/en/2357302"seem not to be helpful. All my scripts or actions are at least used onceper day. And none of them generated an error. Whatever the moment of starting, the script blocks after exactly 2147483647 ms. Best regards, |
Follow us on