Industry Online Support
Technical Forum
11/22/2011 8:34 PM | |
Joined: 4/22/2010 Last visit: 5/3/2024 Posts: 5697 Rating: (713) |
Hello, Well for programming there is a sort of standard, IEC 61131, you can search for that. http://support.automation.siemens.com/WW/view/en/8790932 In case of hardware, i believe every brand has it's own tricks, so there is a big difference. 300 programs should run in a 400, but again the hardware and therefore the (build-in)functions, addressing differ. So some work to do when using a program written for a 300 in a 400. Regards Marcjan |
Problem solved? |
|
Follow us on