10/1/2020 11:41 AM | |
Joined: 8/12/2020 Last visit: 5/18/2021 Posts: 9 Rating: (0) |
hi how can i add other device IEC61850 comunicatin (cid or icd) such as ABB RTU, in digsi 4.92 ? |
10/5/2020 6:48 AM | |
Joined: 6/19/2017 Last visit: 5/3/2024 Posts: 7994 Rating: (163) |
Closed cause question posted twice. The second thread with the subject how can connect two RTU together with IEC61850 is published within the conference Meet & Talk. Best regards,Jen_Moderator |
My Forum is the place to personalize your profile, |
|
Follow us on