1/17/2020 8:22 AM | |
Joined: 1/15/2020 Last visit: 3/8/2024 Posts: 1 Rating: (0) |
Hi Guys, I have an issue regarding the behavior of the PLC program for Basic Instruction ADD_R. kindly refer to the attached image for your reference. The output parameter of the instruction is not adding the parameter IN1 and IN2. But upon resetting the value to zero, the instruction works. The issue is how come the ADD_R instruction did not proceed with adding the real number upon reaching the output value 2.09814e+006? well in fact according to the manual it is still within the valid area for a result (+1.17549E-38 < result < 3.402824E+38). ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 01/17/2020 16:44:09New subject after splitting |
|
1/17/2020 5:15 PM | |
Joined: 9/21/2012 Last visit: 4/27/2024 Posts: 3930 Rating: (444) |
#IN1 and that will generate a pulse, every time it's on. Calculation stops, because #IN1 is off. |
1/18/2020 9:12 AM | |
Joined: 10/7/2005 Last visit: 4/28/2024 Posts: 3004 Rating: (1046)
|
I'd say it is for the same reason as the answer that was given in the original thread from which this post was split from which is: Have a look at the FAQ below guys, it will (should) answer all your questions: |
Cheers |
|
Follow us on