Industry Online Support
Technical Forum
11/30/2012 1:46 PM | |
Posts: 378 Rating: (47) |
Hello Attila_666, noit sure if i understand you correct. But i think you don´t need the gsd, you need the hsp for tia v11, which can be downloaded under the following link http://support.automation.siemens.com/WW/view/en/54164095 Best regards Bilao |
11/30/2012 2:24 PM | |
Joined: 9/27/2006 Last visit: 4/27/2024 Posts: 12257 Rating: (2665) |
Hello Attila; Bilao is right: a gsd file is required only when you want to setup a Profibus-DP slave. Since the Siemens CPUs are already integrated as potential DP slaves in the form of metadata in the Profibus catalog of HWConfig, a gsd file for a Siemens CPU is only needed when you want to integrate the CPU as a slave to a non-S7 Profibus configuration software. Look for your HSP as suggested earlier if you want to update the hardware catalog of the TIA Portal. See the following link: STEP 7 (TIA Portal) V11 Support Packages for the hardware catalog in the TIA Portal Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 11/30/2012 2:27 PMSorry Bilao, the link provided is the same as yours. |
|
Follow us on