12/18/2020 2:40 AM | |
Joined: 10/22/2015 Last visit: 6/7/2024 Posts: 23 Rating: (4) |
Hello, I added more characters for SQL queries in this application example provided in this link: we have a limitation on the length of a string for queries, however if you need a larger query, I added 3 more strings. Before the block had only 1 string for query, now it has 4 strings, which are automatically concatenated, just write the query and when you reach the 254 character limit of the first string, keep writing in the next string. This is very useful for large queries. I tested it and it's working. I hope to help someone! Attachment109779336_SQL_S7_1500_CODE_V20.zip (832 Downloads) |
Last edited by: Jen_Moderator at: 12/18/2020 11:58:25Optimized link. |
|
This contribution was helpful to8 thankful Users |
12/16/2022 5:24 PM | |
Joined: 4/28/2015 Last visit: 6/29/2024 Posts: 1 Rating: (0) |
For the V31 library do you have the same? Thanks a lot |
Follow us on