11/17/2023 6:43 PM | |
Joined: 12/18/2014 Last visit: 7/1/2024 Posts: 33265 Rating: (4116)
|
And what is the range of the sensor signal? 0 to 20mA? Or 4 to 20mA? |
11/17/2023 7:11 PM | |
Joined: 12/18/2014 Last visit: 7/1/2024 Posts: 33265 Rating: (4116)
|
Try this. But make sure that the AQ1 is setting to 4-20mA. |
11/17/2023 7:43 PM | |
Joined: 12/18/2014 Last visit: 7/1/2024 Posts: 33265 Rating: (4116)
|
Otherwise. Please upload your program. |
11/18/2023 5:08 AM | |
Joined: 4/14/2023 Last visit: 6/24/2024 Posts: 8 Rating: (0) |
This is the program that o tried to do, but I can't replicate the same mathematical operation as in your file. I have already configured the input/output to the correct ones on for the logo AttachmentConversion_Range.zip (404 Downloads) |
Follow us on