6/5/2017 11:08 AM | |
Joined: 11/16/2006 Last visit: 3/1/2024 Posts: 92 Rating: (14) |
After installing of incompatible WinCC Flexible 2008 SP3 Step7 V5.6 on Window 10 x64 I have error message https://support.industry.siemens.com/tf/ru/en/posts/error-during-installation-of-step-7-ver-5-5/101864?page=0&pageSize=10 when start Step7
Running installed Step7 V5.6 with Administrator Rights solved this start problem. В случае появления подобной ошибки при запуске Степ7 - запустите его по меню правой кнопки от Имени Администратора.
------------------------------------------------------------------------------------------ |
Last edited by: Simaticov at: 6/5/2017 11:12:03 AMLast edited by: Min_Moderator at: 6/6/2017 12:15:21 PMNew subject after splitting |
|
This contribution was helpful to2 thankful Users |
2/1/2018 2:01 AM | |
Joined: 10/9/2015 Last visit: 4/26/2024 Posts: 9 Rating: (0) |
thank you very much. |
2/13/2018 7:58 AM | |
Joined: 3/9/2009 Last visit: 4/29/2024 Posts: 4 Rating: (0) |
Thank you also for this "solution". Is Siemens working on a fix for this problem? |
6/18/2018 7:51 AM | |
Posts: 1 Rating: (0) |
i have also the same issue. OS: Windows 10 x64bit it's working when i tried to run it as administrator. but's not the proper solution. needs to fix this issue. |
Follow us on