4/15/2019 8:33 AM | |
Joined: 9/24/2010 Last visit: 10/12/2024 Posts: 27 Rating: (1) |
thanks a lot for answer i killed the process "sqlservr.exe" in Windows Task Manager and then start archive function it ok but after making restart and making another archive function the same error Archive Project (256:67):OS(1)RT.ldf' because it is already being used by another application. OS(1)\OS(1)RT.mdf' because it is already being used by another application. OS(1)\OS(1)Tlg.ldf' because it is already being used by another application. so how to fix that and i also made 1. Stop the WinCC server in SQL enterprise manager 2. Archive 3. Enable server it make archive but after restart not working the same error so how to make permanent solution for that problem as it was working good before ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 4/15/2019 2:42:47 PMNew subject after splitting |
|
Follow us on