8/5/2020 4:52 PM | |
Joined: 6/4/2018 Last visit: 12/13/2023 Posts: 3 Rating: (0) |
I am using sick dme4000 ssi absolute encoder with smc30. I have done following setting P0407[1]-100000 nm (resolution is 100 um) P0422[1]-100000 nm G1_XIST1-4 G1_XIST2-4 Positioning data length -24bits Problem observed is everytime after power on off need to perform referencing. Reference point set bit turns off after power on off. Referencing gets lost after power on off ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 08/06/2020 09:42:55New subject after splitting |
|
8/6/2020 5:35 PM | |
Joined: 10/11/2006 Last visit: 12/20/2024 Posts: 5974 Rating: (820)
|
Hello, maybe you forgot to adjust your absolute encoder. There is a SIMATIC Function block available, which you can use for adjusting the absolute encoder, in case you use a SIMATIC S7-1200 or 1500 CPU. https://support.industry.siemens.com/cs/ww/en/view/109760317 |
With best regards, |
|
12/8/2022 10:39 AM | |
Joined: 4/9/2014 Last visit: 5/24/2024 Posts: 4 Rating: (0) |
After referencing save RAM to ROM |
Follow us on