3/26/2016 11:52 AM | |
Posts: 4 Rating: (0) |
Hello and Greetings to all, I would like to ask for help regarding an error I have encountered during preventive maintenance, I did some cleaning and dusting of the control panel and after the cleaning procedure,I switched the power ON, and the PLC's are in red light and the unit S7-300 is lighting on "STOP", all of the switch butttons on the control panel are not functioning, My question is " What could be the possible reason of this type of error? and What should I do to in order to correct this error? hence If I may require, please send on reply, a step by step procedure on what should be done! Thank you in advance! ------------------------------------------------------------------------------------------ |
Last edited by: StaffSgt. at: 3/26/2016 1:50:14 PMLast edited by: Min_Moderator at: 3/29/2016 12:18:55 PMNew subject after splitting |
|
Follow us on