1/13/2018 7:57 PM | |
Joined: 1/12/2018 Last visit: 7/29/2024 Posts: 16 Rating: (0) |
Hello I have a problem with sinumerik, in HMI appears an alarm, 25000, Hardware fault of active encoder, it get active when I try to reference the axis, to be sure that both measurement systems are measuring, servo encoder and linear encoder, I see the screen where appears both measurement, I move by hand pushing and pulling the axis and te relation of both system are almost the same 4 microns of diference, but the problem appears at the moment of move the axis by control. First time that alarm appear was when I take away the servo of its housing, and I think maybe is the cable, but I have the doubt because I can see the values of their position (servo and linear encoder) in the screen. Can any body help us Taking advantage of this I like to know if someone has a manual or knowledge about Acramatic 2100 control by siemens Best Regards ------------------------------------------------------------------------------------------ |
Last edited by: Alex.Landa at: 1/13/2018 7:58:05 PMLast edited by: Jen_Moderator at: 1/15/2018 1:09:53 PMNew subject after splitting |
|
Follow us on