Industry Online Support
Technical Forum
8/18/2010 8:17 AM | |
Posts: 1 Rating:
|
Hi, I have the same A17 when powering up a Simovert VC (6SE7031-0TE60). The A17 alarm would clear about 5mins after the drive was powered up and the status would change to 9 (drive ready). However, when we attempted to drive the motor we got F17. After the motor & cables meggered ok the whole drive was changed and parameters uploaded. The drive is now running ok. Our employer would like us to identify the faulty component, would you suggest swapping the CUVC card or possibly swap around IGBTs to see if we get F26?
Splitted from Warning 17 MasterDrive VC. |
Last edited by: O_Moderator at: 8/18/2010 9:56 AMnew subject after splitting |
|
8/19/2010 5:48 AM | |
Posts: 3 Rating:
|
Do you have F26 Fault with A17? If so, maybe you have the same problem as I had in SimovertMasterdrive. I change PSU2 board to sole this problem. Se also https://www.automation.siemens.com/tf/WW/en/Posts/43903#top |
11/22/2016 1:07 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4767 Rating:
|
New question published by rameezit is split to a separate thread with the subject Alarm 17 when I connected a new IVI card. Best regards |
Follow us on