5/21/2014 7:59 PM | |
Joined: 11/21/2007 Last visit: 12/23/2024 Posts: 2325 Rating:
|
Hello PDGANGANI Unfortunately I do not have WinCC Professional V11 installed currently. Will try to install and check over next couple of days. BTW is there the Template Option in WinCC Professional V11 ( As in WInCC Advanced V11 ).. if so then you can use it. Yes,you can configure in all screens .. but then it is quite cumbersome ... Hope this helps Cheers Navnag |
There is no such thing as the last bug in a program |
|
5/21/2014 8:20 PM | |
Posts: 165 Rating:
|
Hello Navang, Right now i can't find Template option like TIA Advance V11 or Wincc Flexi. Thanks for quick reply and support, Once you install TIA V11 Professional then keep informed me |
Follow us on