2/27/2019 12:56 PM | |
Joined: 10/26/2011 Last visit: 5/3/2024 Posts: 761 Rating: (190)
|
Hi mtn_bzkrt, There is a FAQ available with the following title: How do you delete non-acknowledgeable messages in the PCS 7 OS Runtime or WinCC Test this once, it should solve the problem.
|
SIMATIC PCS 7 - Overview |
|
This contribution was helpful to1 thankful Users |
2/28/2019 4:10 AM | |
Joined: 3/30/2012 Last visit: 4/14/2024 Posts: 18 Rating: (1) |
Many thanks! I have the same problem in PCS 7 V8.2 SP1. I will try it. |
3/7/2019 1:38 PM | |
Posts: 17 Rating: (0) |
Hello chenway Does the problem continue in PCS 7 V8.2 SP1? Did you find a solution? |
3/28/2019 8:59 AM | |
Joined: 5/3/2017 Last visit: 4/19/2024 Posts: 673 Rating: (216) |
Hello mtn_bzkrt, the FAQ How do you delete non-acknowledgeable messages in the PCS 7 OS Runtime or WinCC should work at WinCC Version 7.4 SP1 and higher. At the SP1 Siemens had made changes in the WinCC to delete these messages. with regards |