4/13/2017 12:15 PM | |
Posts: 1 Rating:
|
Hi all, I am using 'Program Alarms' which are defined under 'PLC supervisions & alarms'. Here I can link a 'Program Alarm' to an alarm class. To show the active 'Program alarms', I use the Alarm Viewer from the Toolbox. Using the Alarm Viewer in an HMI screen, I am able to choose which alarm class have to be shown in the alarm viewer. Properties > General > Display > enable alarm classes. However, using the same Alarm Viewer in a faceplate, I do miss a couple alarm classes which actually have to be shown in the Alarm viewer. How could I add the missing alarm classes in the Alarm Viewer when I use it in a faceplate? Suggestions would be valuable! Geert Mulder TIA Portal V14
AttachmentAlarm viewer in HMI screen and Faceplate.docx (172 Downloads) |
4/24/2017 9:09 AM | |
Posts: 648 Rating:
|
Dear geertmulder, this application example could be helpful for you: https://support.industry.siemens.com/cs/ww/en/view/68014632 With best regards rh1990 |
Follow us on