Industry Online Support
Technical Forum
3/28/2009 9:37 AM | |
Joined: 4/10/2006 Last visit: 10/18/2024 Posts: 934 Rating: (2) |
Hallo Rodrigo N. I had the same problem with a OP177B ... I do not know if the philosophy is the same for the MP277 but can not bring up the alarm ONLY when ON...the same warning also appears when going to OFF: /tf/WW/en/Posts/28183#top As concerns the recording in a log file, nell'MP277 think you can use the scripts Bye-Bye Roby |
Setting of my PG M6 Siemens |
|
Follow us on