3/12/2019 1:49 PM | |
Posts: 1 Rating:
|
we are using CPU 6ES7 414-3XJ04-0AB0 ( Firmware Ver. 4.1.0) and it is working fine for the last 8-years. Recently we have observed the problem that all LED's on CPU are blinking and lost communication with all connected devices. If we stop the power supply module and restart again after few seconds, then it is working ok and after few hours (some time) same thing is happening( i.e. All LED's Blinking), some times it works for 3 to 4 days and then happening the same. So we replaced with new CPU module( 6ES7 414-3XJ04-0AB0) and now it is working fine for the last 4- months. can anybody suggest what will be the problem with old-CPU-Module. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 3/13/2019 11:33:13 AMNew subject after splitting |
|
3/19/2019 7:27 AM | |
Joined: 12/9/2010 Last visit: 10/8/2022 Posts: 623 Rating:
|
Hi AutoGen_1010859, The CPU needs maintenance. Please share diagnostics buffer log. |
If you like the comment, rate it (right top) or thank it (left bottom). |
|
3/27/2019 10:37 AM | |
Joined: 1/1/2017 Last visit: 7/1/2024 Posts: 331 Rating:
|
Hi AutoGen, I think that the CPU needs firmware update. Regards OmKris |
Follow us on