1/16/2020 10:25 AM | |
Joined: 5/11/2019 Last visit: 12/18/2022 Posts: 3 Rating: (0) |
Hi.. I also have the same issue with TIA V14 SP1. While opening ALM, it is showing " cannot start access-protection components". I tried reinstalling ALM V6.0 SP1. still not working Also tried "Run as administrator". System is 64bit OS running Windows 7 professional. could anyone help? ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 01/16/2020 17:45:25New subject after splitting |
|
4/18/2024 5:52 AM | |
Joined: 7/18/2023 Last visit: 4/23/2024 Posts: 9 Rating: (0) |
I have the exact same error. Any fixes other than disabling Win Defender? |
Follow us on