5/1/2016 6:36 PM | |
Joined: 9/18/2013 Last visit: 2/20/2024 Posts: 203 Rating:
|
Hello, I think this link will be very helpful |
5/1/2016 6:58 PM | |
Posts: 17 Rating:
|
hello thank you for your help ; but this solution is made just to send SMS it may be helpful but i need that informations wich cames frome an ET200M get traited by the S7-400 and goes back to the ET200M
|
5/2/2016 6:12 AM | |
Joined: 11/21/2007 Last visit: 3/31/2025 Posts: 2326 Rating:
|
Hello The following links would be useful for you : Getting Started with Industrial Remote Communication Wireless Communication of S7‑300 Stations with TeleControl Server Basic V3 How do you parameterize the GSM modem MD720-3 for use with SINAUT ST7? How can you prevent the PROVIDER from automatically disconnecting the GPRS connection between a MD720-3 modem and SINAUT MICRO SS? How can you safely change between GPRS mode and AT mode for SINAUT MD720-3? Which firewall rules should you configure for the GPRS router MD740-1 in order to have access to the Internet with the PG/PC from the LAN of the MD740-1? Hope this helps Cheers Navnag |
There is no such thing as the last bug in a program |
|
Follow us on