7/12/2019 12:32 PM | |
Joined: 6/20/2010 Last visit: 7/20/2024 Posts: 96 Rating:
|
Hi Ixo again, I have a two Logo 0A07 standard, I just use your example two years ago; now there is a analogic comunication between two LOGO 7, I have a problem when disconect one of them becouse the anaglogic output frozen and always the other one receive the last conection. I want advise to one of them that the comunication fail, and the other one use another way of program. I only change the phisical analog output, but not analog inside. Thanks in advance. https://www.dropbox.com/s/l9i7qy2fkzbmgxx/VID_20190712_114345.mp4?dl=0 ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 07/15/2019 06:04:01New subject after splitting |
|
7/14/2019 9:42 AM | |
Joined: 6/20/2010 Last visit: 7/20/2024 Posts: 96 Rating:
|
I´m going check again the real LOGO`s |
7/19/2019 6:23 PM | |
Joined: 12/18/2014 Last visit: 7/25/2024 Posts: 33414 Rating:
|
Then show us your UDF. |
7/19/2019 6:56 PM | |
Joined: 6/20/2010 Last visit: 7/20/2024 Posts: 96 Rating:
|
I made an easy program inside, I just put a picture inside the Dropbox link, anyway here is a pdf.
AttachmentUDF_BIT_VIDA.pdf (137 Downloads) |
Last edited by: Otobit at: 07/19/2019 19:03:18 |
|
7/19/2019 7:41 PM | |
Joined: 12/18/2014 Last visit: 7/25/2024 Posts: 33414 Rating:
|
In attachment an example for exchanging life bits between two 0BA7. And also using diagnostic bit in both LOGO!s. AttachmentLife_bit_exchange_between_two_LOGO!_0BA7.zip (128 Downloads) |
7/19/2019 7:48 PM | |
Joined: 6/20/2010 Last visit: 7/20/2024 Posts: 96 Rating:
|
Thanks a lot Ixo, it`s better way to solve the problem.
|
This contribution was helpful to
1 thankful Users |
Follow us on