8/5/2008 12:14 PM | |
Posts: 3 Rating: (0) |
Would some one please tell me,why Analog countis 27648? |
8/5/2008 1:21 PM | |
Posts: 3 Rating: (0) |
Sorry, I couldn't elaborate my question well. I wann ask why siemens has standardised analog input countfrom 0 to 27648? |
8/5/2008 2:31 PM | |
Joined: 7/16/2006 Last visit: 1/2/2024 Posts: 1502 Rating: (176) |
You have many Part. This are all Analog Inputs 0..20mA 0...5Volt 0...10Volt 0...400Ohm PT100 Sensor (100hm 20°C) PT1000 Sensors (1000Ohm 20°C) NiCrNi THermoelemente Wich number shold by an 10Volt or 5 Volt ? and so on. And all Units have as Example 27648 is 100% from all Units (Normaly) 0...5Volt 100% 27648 0..10Volt 100% 27648 I hove that ist the answer for your question. |
Karl |
|
3/4/2010 7:14 PM | |
Posts: 1 Rating: (0) |
Can someone please post a link to the manual where the above table can be found. |
3/4/2010 8:17 PM | |
Joined: 9/27/2006 Last visit: 12/20/2024 Posts: 12307 Rating: (2695) |
Hello TWW; |
Follow us on