4/22/2018 11:46 PM | |
Joined: 4/28/2015 Last visit: 3/15/2024 Posts: 26 Rating: (1) |
Hello, I have a program which needs to read the temperature of meat @ 72 degrees and then trigger the next stage process. i have to use the pt100 in place, which I've added a transmitter (https://www.amazon.co.uk/gp/product/B00GN6X25U/ref=oh_aui_detailpage_o02_s00?ie=UTF8&psc=1) with two 1kOhm resistors to change the analog input from 4-20mA to 0-10V (1-10V) DC. My program reads the temperature, but it isn't changing, i'm not sure i have the correct settings. I have just read this article (https://support.industry.siemens.com/tf/gb/en/posts/0-10v-input-signal/179792/?page=0&pageSize=10) and changed the minimum / maximum settings of the analog amplifier to -50 to 150. Please could someone confirm i have configured the analog amplifier correctly? Thank you. Andy AttachmentSteam Oven Live.zip (306 Downloads) |
Last edited by: AutoGen_911641 at: 4/22/2018 11:47:26 PM |
|
4/27/2018 7:19 PM | |
Joined: 4/28/2015 Last visit: 3/15/2024 Posts: 26 Rating: (1) |
Hi ixo65, thanks for reply, program attached. a decimal would be great ideally AttachmentSteam Oven Live new.zip (252 Downloads) |
Follow us on