6/16/2023 8:11 AM | |
Joined: 4/20/2023 Last visit: 7/17/2024 Posts: 33 Rating:
|
Hello, I hope this message finds you well. I have a masterdrive 6SE7087. I wanted to control it via ET200SP and 1215C DC/DC/DC. Digital input and output(start, stop, no fault, turning left, turning right) worked perfectly fine. For analog input and output, it's written in the manual of masterdrive that it works with 0-20mA however when I set the channel to 0-20mA it didn't work at all, but when I changed it to 4-20mA it worked which was strange. For the analog output of masterdrive (Tourqe and Actual speed) I didn't get to any right value. I am using AI 8xi 2-/4-wire BA for analog input of ET200SP. I tried 2wire and 4wire connection with current measurment of 0-20mA and 4-20mA but it didn't work out. The masterdrive has been set for current output and input. The wires are also twisted pair. Attached you'll find the wiring and manual. Thanks in advanced. AttachmentMasterdrive.zip (484 Downloads) |
6/16/2023 12:16 PM | |
Joined: 3/25/2008 Last visit: 7/8/2024 Posts: 191 Rating:
|
hello, how do you set the switches? And how the parameters Aout.
AttachmentCUVC_aout.zip (435 Downloads) |
Follow us on