7/10/2013 5:38 PM | |
Joined: 1/21/2013 Last visit: 6/6/2024 Posts: 4620 Rating: (705) |
Hi 10leiva, Send us your hardware configuration. |
7/10/2013 6:10 PM | |
Joined: 7/3/2013 Last visit: 2/15/2023 Posts: 11 Rating: (0) |
the analog inputs are in the hardware config4.jpg
AttachmentHardware config1.zip (325 Downloads) |
7/10/2013 6:49 PM | |
Joined: 4/19/2008 Last visit: 6/6/2024 Posts: 1525 Rating: (159) |
Hello 10leiva, Have a look on the Wiring Detail on the Manual, have you done the wiring same way? 2AI I 2WIRE ST analog electronic module (6ES7134-4GB01-0AB0) |
Ammy |
|
7/10/2013 7:48 PM | |
Joined: 7/3/2013 Last visit: 2/15/2023 Posts: 11 Rating: (0) |
Yes. "+" to "1" and "-" to "2", (IW2000). "+" to "5" and "-" to "6", (IW2002).
|
Follow us on