10/8/2022 9:18 AM | |
Joined: 3/14/2008 Last visit: 7/12/2024 Posts: 2076 Rating:
|
Hi, It helps if you can show some print screens and more info on the used module driver (there are several). So please attach screens (online mode) and hardware config (you have to parametrize the channel for like 0-20mA or 4-20mA etc.) Maybe there is a wrong setting. |
If I could help you, you can use the RATE button. Thank you. |
|
10/10/2022 7:02 AM | ||||||||||||||||||||||||||||||||||||
Joined: 2/6/2015 Last visit: 6/25/2024 Posts: 22 Rating:
|
Hi Oreca,
Attachmentsnaps.zip (282 Downloads) |
|||||||||||||||||||||||||||||||||||
10/11/2022 5:45 AM | |
Joined: 3/14/2008 Last visit: 7/12/2024 Posts: 2076 Rating:
|
Hi, It makes sense. You are using PLCSim to simulate values. The module driver connections are created so the program expects real diagnostic data from the hardware, which you don't have.
|
Last edited by: Oreca at: 10/11/2022 05:46:34If I could help you, you can use the RATE button. Thank you. |
|
10/11/2022 12:43 PM | |
Joined: 2/6/2015 Last visit: 6/25/2024 Posts: 22 Rating:
|
Hi Oreca, Thanks for reply. You mean from PLCSIM we can not see output value for IO address? |
Follow us on