10/28/2018 12:42 PM | |
Joined: 11/15/2015 Last visit: 7/13/2024 Posts: 179 Rating: (28) |
Hello Hama salih, You are very welcome to Forum, Actually when you make a tank zero, by PDM Software (process device manager) make upload to PG for the device settings and then increase the lower value for the scale output of the device and then download again to the device until you get the actual (reading you can monitor that at SCADA).. if the device DP or PA you can use PDM from hardware configuration.. Or you can download it separately and then by CP like CP1157 you can communicate with the device. IF the device PA you can use DP\PA coupler. Regards ========================================================= Look for alternative not for the correct answer.... |
Last edited by: ahmed alqubati at: 10/28/2018 12:46:02 PMLast edited by: ahmed alqubati at: 10/28/2018 12:50:34 PMLook for alternative not for the correct answer...if this is helping you rate it. |
|
10/28/2018 4:23 PM | |
Joined: 1/21/2013 Last visit: 6/6/2024 Posts: 4620 Rating: (705) |
Hello, how is your program? can you share with us? |
10/29/2018 7:17 AM | |
Joined: 11/15/2015 Last visit: 7/13/2024 Posts: 179 Rating: (28) |
Hello, The software PDM you can find inside CD for PCS7 any version. have a look at the attached file how to use it.. Regards, ========================================================= Look for alternative not for the correct answer.... AttachmentPDM.pdf (120 Downloads) |
Look for alternative not for the correct answer...if this is helping you rate it. |
|
Follow us on