8/2/2023 4:40 AM | |
Joined: 10/15/2022 Last visit: 7/24/2024 Posts: 66 Rating: (2) |
Hi, LOGO! enthusiasts. Another demo, this time for analog ramp. The program automatically changes the speed of the ramp "on the fly" between four speeds, depending on the level reached. The level starts at zero and goes up to a one thousand and then goes back to zero and so on. An analog ramp can be used, for example, to smoothly change the voltage Important to know! When simulating program, ramp speed not changing automatically. Tested on the real controller (6ED1052-1MD08-0BA1, with firmware 1.83.02). As usual, three files in the zip file (program, scheme and description). Andrus AttachmentAnalog ramp demo.zip (589 Downloads) |
Last edited by: Andrus_Saar at: 08/08/2023 16:44:19 |
|
This contribution was helpful to1 thankful Users |
Follow us on