11/3/2015 3:46 PM | |
Joined: 12/18/2014 Last visit: 4/28/2024 Posts: 32898 Rating: (4067) |
Look at attachment. |
11/3/2015 3:55 PM | |
Joined: 8/5/2015 Last visit: 9/20/2021 Posts: 120 Rating: (3) |
i try it of 4 mA i get 0 % but in 6mA i have 100 |
11/3/2015 5:25 PM | |
Joined: 12/27/2006 Last visit: 4/27/2024 Posts: 1196 Rating: (113) |
Let us show what parameters you have set in the analog block. Post your programm, and we can see whats going wrong. |
11/3/2015 6:29 PM | |
Joined: 12/18/2014 Last visit: 4/28/2024 Posts: 32898 Rating: (4067) |
Here is the file, for example.
AttachmentSchaltplan1.zip (156 Downloads) |
11/4/2015 7:32 AM | |
Joined: 2/12/2014 Last visit: 5/28/2023 Posts: 158 Rating: (0) |
is the value whne you inject 6mA maximum? |
11/4/2015 4:37 PM | |
Joined: 12/18/2014 Last visit: 4/28/2024 Posts: 32898 Rating: (4067) |
Here's a little more Information.
AttachmentLogo overview analog voltage current units.pdf (185 Downloads) |
Follow us on