4/20/2012 7:59 PM | |
Joined: 3/21/2006 Last visit: 11/1/2024 Posts: 10229 Rating: (1181) |
How do you set up a teleservice connection to LOGO! with an analog modem via the telephone network? |
4/20/2012 9:50 PM | |
Joined: 1/5/2007 Last visit: 4/7/2023 Posts: 1690 Rating: (580)
|
Hello, yes, the models 0BA6 and their previous models have a front-sided RS-232 interface and can connected via a modem at this interface. Over this way the I/O-Status can be read and send over the telephone network. |
==> Meine TAG-Listen: "deut." |
|
This contribution was helpful to1 thankful Users |
4/23/2012 10:25 AM | |
Posts: 11 Rating: (0) |
Thanks for the answer, but just to be sure to have understood completely: - not even using an analogic modem with a RS-232/ethernet adapter? |
4/25/2012 11:07 AM | |
Posts: 495 Rating: (58) |
You can use the Teleservice module modem together with the teleservice adapter IE Basic from S7-1200. This could work. |
Follow us on