5/29/2018 12:32 PM | |
Posts: 200 Rating: (6) |
Hi I have program running that has a analogue signal input from a duct sensor the program may run for around a hour and then the Analogue value will jump from around 20 to above 50 and then cause the program to stop the value is displayed on a KTP700 HMI and when goes over 50 displays #### instead of the numbers and then shuts then stops the program i am not sure why this is happening and wounder if someone can see anything within my software on why this would be happening i have also added a pic of the sensor settings guide AttachmentSoftware.zip (205 Downloads) |
Last edited by: andrewdaw1978 at: 5/29/2018 12:37:54 PM |
|
5/29/2018 12:38 PM | |
Posts: 200 Rating: (6) |
screen shots
AttachmentDoc1.pdf (228 Downloads) |
5/29/2018 3:18 PM | |
Joined: 10/20/2015 Last visit: 5/21/2024 Posts: 94 Rating: (19) |
Yes, that too.. I missed that part welldone ixo
|
Follow us on