9/22/2022 10:00 AM | |
Joined: 7/23/2021 Last visit: 8/16/2023 Posts: 5 Rating: (0) |
Hello, have problem with analogic output card. When try via HMI give 10V to output the module his give 0V. I know about range 0..27648. The hardware settings was correct. Have PLC CPU 315-2 PN/DP. Firmware version is 3.2.17. Try create new program for testing the AO and same result. According this manual verify output voltage:Analog output module SM 332; AO 4 x 12 Bit; (6ES7332-5HD01-0AB0) - SIMATIC S7-300 S7-… - ID: 8859629 - Industry Support Siemens Try measure voltage on pin 3 and 6. 7 % 10. Have attached image configuration and test project. AttachmentTest_AO.zip (571 Downloads) |
Last edited by: EasyS at: 09/22/2022 12:49:01 |
|
Follow us on