6/30/2013 11:27 AM | |
Posts: 559 Rating: (87) |
Yes there is no problem in Logic. The problem must be somewhere at your hardware side. Please check it out or change the channel address & then check. |
8/8/2013 8:07 AM | |
Posts: 81 Rating: (2) |
Hello, I am measuring mA on multimeter. I am direclt forcing value in QW. But still it is not genrating any kind of value on my multmeter. Is my settings are correct with this module?? Dear experts plz resolve this issue as soon as possible. regards, manoj
AttachmentAO.pdf (199 Downloads) |
8/8/2013 8:30 AM | |
Joined: 1/21/2013 Last visit: 6/6/2024 Posts: 4620 Rating: (705) |
Hi MANOJ.N, In which terminals are you measuring the current? Send us a diagram of your connections on the board. |
8/8/2013 8:51 AM | |
Posts: 81 Rating: (2) |
Hello from this diagram,I am getting confused. On which terminal I have to measure current?? regards, manoj
|
8/8/2013 9:02 AM | |
Posts: 81 Rating: (2) |
Hello, Yes i am measring current on the same terminal 3 for +ve & 6 for -ve terminal. regards, manoj
|
8/8/2013 10:25 AM | |
Joined: 1/21/2013 Last visit: 6/6/2024 Posts: 4620 Rating: (705) |
Hi MANOJ.N, You have applied a load of this measurement? |
Follow us on