2/15/2023 2:56 PM | |
Joined: 11/4/2022 Last visit: 7/5/2024 Posts: 17 Rating: (0) |
Hello, I have one ES and 2 Single server OS and one AS. My project is Multiproject. I downloaded my server OS from ES to Server Pc. After that I started my project on Server PC, Everything is fine but I saw that my interlock button where is in Faceplate was disabled. Also for test, I started Eng station scada, everything are working fine. There are a lot of topic regarding that but There is no clear solution. I want to share with you some links that I thing regarding that at following. https://support.industry.siemens.com/forum/WW/en/posts/interlock-permission-protect-are-grayed-out-and-faceplate-jump-is-not-showing/226384 https://support.industry.siemens.com/forum/WW/en/posts/interlock-permission-button-disable-in-os/227315 https://support.industry.siemens.com/forum/ww/en/posts/pcs7-8-2-sp1-not-able-to-operate-the-interlock-button/244340 Attachmentsreenshots.zip (468 Downloads) |
2/16/2023 6:08 AM | |
Joined: 11/4/2022 Last visit: 7/5/2024 Posts: 17 Rating: (0) |
Is there somebody that is to help me?. I think that is a chronic problem. |
2/19/2023 6:05 PM | |
Joined: 11/4/2022 Last visit: 7/5/2024 Posts: 17 Rating: (0) |
Really My problem is continue.. if anyone has an idea about my problem, can he share with me? |
2/20/2023 2:56 PM | |
Joined: 11/4/2022 Last visit: 7/5/2024 Posts: 17 Rating: (0) |
Hello Molthoff, I checked my Server project on ES. I coulnt problem fro english language. because my computers, ES and OS is English. Nevertheless I will copy to other language column. I added my screenshot. What you think about my interlock button disable in motL or ValveL faceplates (I added also at attach)
AttachmentInterlock button disable.zip (529 Downloads) |
Follow us on